Often there are long set-up times and unnecessary machine downtimes due to numerous temperature regulation connections. Not only time loss but also quality issues can also result through possible coupling errors. Meusburger offers the perfect solution for optimising set-up times with their system EU & USA multi couplers.
Short set-up times
The various multi couplers from Meusburger make it possible to connect the temperature control circuits in just one step. Through the central connection customers benefit from optimised set-up times of the temperature regulation components of, for example, 20 minutes down to 20 seconds. Errors such as mixing up the hoses can also be avoided. This makes set-up processes not just fast, but also easy and reliable. Time savings start already in the design phase thanks to clear selection, CAD data and ordering at the press of a button, as well as delivery from stock.
System changeover - but how?
It makes sense to use the same coupling profile that is currently in use. This allows coupling to the multi coupler on the mould parallel to the changeover of the individual hoses on the machine. For this purpose, Meusburger offers the multi coupler in the systems EU (E 2861 / E 2871), USA (E 2862 / E 2872) and RMI-Stäubli (E 2830 / E 2833). In mould making, the pressure test can then also be carried out with single couplers. In the Meusburger range, the multi couplers are available with free flow or with valve. Due to the modular design, the connection of the hoses is possible by means of different nozzles or threads.
Further advantages
By preheating the mould before the changeover, the time until the first good part can often be significantly reduced again. Due to the simple connection option, the multi coupler is also ideal in this situation. With frequent mould changes, downtimes can be greatly reduced and the number of skilled personnel required can be significantly minimised.
The Meusburger multi coupler is the optimal solution for frequent mould changes.
Prova la nostra nuova versione della sezione “Il mio account“
Scoprite sin da subito la nostra nuove sezione “Il mio account” e approfittate dei numerosi vantaggi.
La nuova sezione “Il mio account” vi consente ora di accedere direttamente al livello successivo del nuovo portale della Meusburger. Qui trovate tutte le informazioni e i vantaggi del portale.
Scoprite sin da subito la nostra nuove sezione “Il mio account” e approfittate dei numerosi vantaggi.
La nuova sezione “Il mio account” vi consente ora di accedere direttamente al livello successivo del nuovo portale della Meusburger. Qui trovate tutte le informazioni e i vantaggi del portale.
Mantieni la selezione
Beta
Nuova versione
Visualizza tutti i dati sugli ordini
Tracking delle spedizioni per tutte le consegne parziali
Cerca e filtra gli ordini
Semplice gestione dei reclami e delle restituzioni
Prova la versione
I dati sugli ordini sono visibili per un massimo di 90 giorni
Tracking delle spedizioni per le consegne parziali