Reliable demoulding of complex injection moulded parts
08.11.2016, Costruzione stampi
The compact ejector accelerator from Meusburger is the ideal device for the safe and targeted ejection of complex parts: a single ejector is additionally accelerated by which snagging of the injection moulded part is avoided. The injection pressure is absorbed by the ejector base plate thus the ejection accelerator does not bear any load and has a longer service life. Due to the small component size a flexible positioning of the ejector accelerator in the ejector set is also possible when retrofitting.
The E 1522 Ejector accelerator from Meusburger optimises the smooth ejection of injection moulded parts. With the newly developed component targeted control of the ejection process is possible. Through the additional acceleration of a single ejector snagging of the injection moulded part is avoided. The acceleration ratio is 1:1.5. Therefore a longer path is achieved with a small stroke. The repositioning of the accelerator does not take place directly through the clamp plate but through a cut to length ejector so the same buffer plates for the ejector set can be used. A further advantage is that the entire injection pressure is absorbed directly by the ejector base plate. As a result the ejector accelerator does not bear any load during the injection moulding process. The three different sizes available allow designers to install ejectors in the diameters of 3 – 11.5 mm at will. The small component size enables a flexible positioning of the ejection accelerator in the ejector set. Therefore the ejector accelerator can also be installed quickly and easily when retrofitting the mould. In order to save design time, the installation space is already included in the CAD data. As usual with Meusburger the new component is available from stock.
Prova la nostra nuova versione della sezione “Il mio account“
Scoprite sin da subito la nostra nuove sezione “Il mio account” e approfittate dei numerosi vantaggi.
La nuova sezione “Il mio account” vi consente ora di accedere direttamente al livello successivo del nuovo portale della Meusburger. Qui trovate tutte le informazioni e i vantaggi del portale.
Scoprite sin da subito la nostra nuove sezione “Il mio account” e approfittate dei numerosi vantaggi.
La nuova sezione “Il mio account” vi consente ora di accedere direttamente al livello successivo del nuovo portale della Meusburger. Qui trovate tutte le informazioni e i vantaggi del portale.
Mantieni la selezione
Beta
Nuova versione
Visualizza tutti i dati sugli ordini
Tracking delle spedizioni per tutte le consegne parziali
Cerca e filtra gli ordini
Semplice gestione dei reclami e delle restituzioni
Prova la versione
I dati sugli ordini sono visibili per un massimo di 90 giorni
Tracking delle spedizioni per le consegne parziali