Contacto

Estaremos encantados de atenderle de lunes a viernes desde las 8:00 hasta las 17:00. Haga clic en este enlace para buscar el interlocutor que le corresponde por zona.

Sede de Wolfurt
+43 5574 6706-0

Sus contactos

Carrito de la compra {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Artículo   Cambiar carrito

Observaciones

Imagen Artículo Unidades Precio por unidad Precio total Precio total con descuento
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben:[{attrPrefix: 'L_', searchPattern: '/...', replacePrefix: '/', replaceSuffix: ''}] }} {{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

     
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

     

Inicie sesión para ver los precios que se le aplican y continuar con el pedido.

Notas de prensa sobre Meusburger

¿Le interesan nuestra empresa y nuestros productos? Entonces está en el lugar adecuado.

TT slide unit now available in two new sizes

24.07.2020, Fabricación de moldes

In addition to the existing sizes with slide surfaces of 12 x 10 mm and 15 x 12 mm, the tried and trusted E 3310 TT slide unit from Meusburger has been expanded with two new sizes with slide surfaces of 8 x 6 mm and 18 x 14 mm. The ready-to-use slide unit reduces overall costs during design and mould manufacturing. In addition, daily work is facilitated through the compatibility of the components and the direct download of CAD data including installation spaces. Small slide units are in particular demand for complex moulds.

With its compact design, the new TT slide unit offers minimum installation spaces. The term ‘TT’ comes from the T-guides in the slide and cotter. This type of guide guarantees optimal force transmission at high injection pressures. The DLC coated slide – out of steel grade 1.2343 with 52 HRC – not only offers a high wear resistance but also best sliding properties. Due to the ESR grade the slides are excellent for mirror polishing. The supplied buffer stops the small slide safely and precisely, even with the highest dynamics. This function can also be implemented directly in the insert or in the cavity plate to save space, which makes previously unrealisable projects such as slides in change moulds possible. In addition, the slide and guide can be installed and removed together.



Installation example of the new TT slide unit in the FW change mould


TT slide unit now available in two new sizes

E 3310 TT slide unit from Meusburger now available in two new sizes

Volver al índice de notas de prensa

Press contact

Should you require further information on this press release or have any questions or comments, please feel free to contact us by email.

Julia Jakob
Comunicación/RR.PP.

+43 5574 6706-1496

Correo electrónico
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
Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Familiarícese de antemano con la nueva sección «Mi cuenta» y disfrute sus numerosas ventajas.

Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Recordar selección
Beta
Nueva versión
Versión actual