Contacto

Estaremos encantados de atenderle de lunes a viernes desde las 8:00 hasta las 17:00. Haga clic en este enlace para buscar el interlocutor que le corresponde por zona.

Sede de Wolfurt
+43 5574 6706-0

Sus contactos

Carrito de la compra {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} Artículo   Cambiar carrito

Observaciones

Imagen Artículo Unidades Precio por unidad Precio total Precio total con descuento
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben:[{attrPrefix: 'L_', searchPattern: '/...', replacePrefix: '/', replaceSuffix: ''}] }} {{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

     
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

     

Inicie sesión para ver los precios que se le aplican y continuar con el pedido.

Notas de prensa sobre Meusburger

¿Le interesan nuestra empresa y nuestros productos? Entonces está en el lugar adecuado.

Proper heat treatment paves the way to success

27.09.2018, Fabricación de moldes Fabricación de herramentales Fabricación de troqueles

Not all stress-relieving heat treatment is the same – because only a proper heat treatment process ensures the desired result in the end. That is why Meusburger has been using its own furnaces for almost 30 years. Meusburger stands for top-quality products – only flawless steel from the best-known steelworks can make it through the quality check. Standard parts that are heat-treated for stress relief are right at the beginning of the die and mould making process chain and form the basis of high-quality moulds and dies.

The heat treatment strength lies in rest

In order to reduce tension in the material to a minimum, in addition to the controlled heating of the sheet metal and the maintaining of the temperature at approximately 580°C, it is especially the uniform cooling that is decisive. At Meusburger the entire heating process, which lasts about 24 hours, takes place in a closed furnace. It is only when stress-relieving heat treatment is carried out correctly that temperature fluctuations and thus the build-up of new tension in the material is prevented, while both the microstructure and the mechanical strength of the material remain unchanged.

Less wear, more capacity

The procedure, from the precise inspection of the sheet metal through to the perfectly executed stress-relieving heat treatment, guarantees low-deformation processing of Meusburger products. The tension in the material is reduced to a minimum. This reduces the load on machines and tools, ensures improved surface quality and lowers the risk of tool breakage. The low warping also ensures that less reworking is necessary, and reduces wear on the cutting tools. The resulting reduced machining time and longer service life allow for free capacity for other tasks.

Proper heat treatment paves the way to success

Meusburger has three furnaces with a total daily capacity of 240 tonnes of steel

Volver al índice de notas de prensa

Press contact

Should you require further information on this press release or have any questions or comments, please feel free to contact us by email.

Lia Klimmer
Head of Department Communications

+43 5574 6706-1516

Correo electrónico
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
Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Familiarícese de antemano con la nueva sección «Mi cuenta» y disfrute sus numerosas ventajas.

Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Recordar selección
Beta
Nueva versión
Versión actual