Nous sommes volontiers personnellement à votre disposition du lundi au vendredi de 8:00 à 17:00 heures. Veuillez cliquer sur le lien suivant afin de trouver les interlocuteurs pour votre région.
10.12.2020, Construction de moules Construction de machines Construction d’outils de découpe
At Meusburger, customers will not only find a very large selection of high-quality P-Standard plates, but also P-Special plates in variable dimensions and various versions. All plates are of course heat-treated for stress relief and machined to very tight tolerances.
Thanks to their 18,000 m² warehouse, Meusburger has a very large selection of P-Standard plates. In addition, the market leader in the area of high-precision standard parts offers special plates with flexible dimensions and various designs. This guarantees that every customer will find the right plate for every project, no matter how specialised. And these are heat-treated for stress relief and in the usual high quality.
High price reliability and short lead time
To ensure that the right range of P-Standard plates for all customers is available, Meusburger reacts quickly to developments on the market and constantly expands their range with sizes in demand. Customers benefit from the P-Standard plates from Meusburger in several ways. P-Standard plates can be ordered in the web shop or also in the offline shop with just a few clicks, and the price display before ordering means that the customers can be sure of exactly what they are spending. The plates are milled in width and length and segment ground in the thickness. They are available in numerous sizes and materials directly from stock. The resulting short lead time guarantees the customer absolute planning security for all projects. Since Meusburger stores the heat-treated for stress relief plates for their customers on a total of 18,000 m², important warehouse space can also be saved.
Flexibility in all areas
In addition to the P-Standard plates, Meusburger also offers customers maximum flexibility with the P-Special plates. With many different versions and variable dimensions, customers have the option of ordering plates customised to the respective project. Despite special machining, Meusburger guarantees fast delivery even for P-Special plates thanks to its modern machinery. Since each individual plate in a special plates order is manufactured according to the customer's requests, the price for each order is recalculated after entering the dimensions, design and material. If a P-Special plate requested by a customer is available from stock as a P-Standard plate, the order is automatically converted to a P-Standard plate.
This goes to show that regardless of whether one of the common sizes of the P-Standard plates is suitable, or more flexibility is required - Meusburger has the right plate for every project. Further information about the variety of plates at Meusburger can be found at: www.meusburger.com.
Si vous possédez déjà des données d’accès au portail Meusburger, veuillez vous connecter ici :
Mot de passe oublié ?
Le nouveau mot de passe généré est en cours d’acheminement et vous devriez le recevoir sous peu dans votre boîte de réception. Nous vous souhaitons une journée couronnée de succès.
Familiarisez-vous préalablement avec notre nouveau section « Mon compte » et profitez de nombreux avantages.
Dès à présent, la nouvelle version de « Mon compte » vous donne également un aperçu direct du niveau supérieur du nouveau Portail Meusburger. Vous trouverez toutes les informations sur le portail et ses avantages ici.
Familiarisez-vous préalablement avec notre nouveau section « Mon compte » et profitez de nombreux avantages.
Dès à présent, la nouvelle version de « Mon compte » vous donne également un aperçu direct du niveau supérieur du nouveau Portail Meusburger. Vous trouverez toutes les informations sur le portail et ses avantages ici.
Enregistrer mon choix
Bêta
Nouvelle version
Accès illimité aux informations relatives à vos commandes
Suivi de toutes vos livraisons partielles
Recherche et filtrage dans la section « Commandes »
Traitement simple de réclamations et de retours
Version actuelle
Accès aux informations relatives à vos commandes pendant 90 jours au maximum
Suivi de certaines livraisons partielles seulement