Die sets Opracování Vestavné díly
More efficiency through standardisation
Standard components have an enormous influence on the cost of a die set. Above all, standardisation offers numerous potential savings - but how exactly?
Read moreComprehensive range of springs for die making
We offer the right spring for every requirement - from very low to extremely high loads. The range also includes perfectly matched accessories for smooth installation of system and elastomer compression springs. The entire selection is immediately available from stock.
Read moreDesky a tyče Opracování Vestavné díly
The right material for every requirement in die making
To meet the different requirements for cutting steels used in die making, Meusburger has a large selection of NE blocks for eroding that cover a wide range of materials - including classic steel for through hardening, high-speed steel, powder metallurgical steel and carbide.
Read moreElements of the strip guide
Many stamping die components such as strip guiding are usually produced in small quantities, which is quite expensive and time-consuming. That is why using standardised components is a good option.
Read moreInovativní ohýbací jednotka pro optimální výsledky
Ohýbací jednotka E 5690 TRIBMATE® EASY ROLLA™, která je k dostání výhradně u firmy Meusburger, snižuje díky valivému tření dodatečné opracování na minimum! Navíc je zdvih neomezený díky válečku s volným uložením.
Read moreVše o plynových pružinách
Choosing the right gas spring among the wide range of products currently available on the market is not easy. Often questions arise such as: How much power do I need? Is this the right size? What do I need to consider for installation or maintenance? And many more. This is exactly where we would like to support you and make it easier for you to choose the right gas spring in the future.
Read moreComparison of guiding types used in die making
Here you will find the areas of application and characteristics of the different guiding elements used in die making.
Read moreAttachments
Through the use of our attachments you can save time and money from the design right through to the commissioning of the die.
Read moreHigh-precision guiding system for modules
A high-precision guiding system serves as the basis of the layout of die modules and is crucial for the quality of your stamped parts.
Read moreActive parts for die set monitoring
Increase process reliability during the stamping process with our precision control devices.This way, damage to the die and falsely stamped parts can be avoided.
Read moreBlock-shaped strip guide, spring-loaded
We are constantly working on further developments with our customers in mind. That is exactly how we developed the following exclusive product in our die making range.
Read moreStandardisation in mould and die making
These days, standardisation along the entire value chain plays a key role in the success of a company. In this article we show you the economic benefits of standardisation with different implementation possibilities especially in mould and die making.
Read moreDie sets Dílenské potřeby Opracování Vestavné díly
Consumables
Cleaning, lubricating, protecting and much more - finding and purchasing the right product for your application can be difficult. With our consumables, you have access to a specially selected range which many of our customers have been using successfully for years.
Read moreDesky a tyče Opracování Vestavné díly
NE – Blocks for eroding
Our blocks for eroding are especially suitable as starting material for the manufacturing of cutting elements and die plates. Due to the different requirements and materials that our customers work with, we have the right material for a wide variety of applications.
Read moreDesky a tyče Opracování Vestavné díly
Material grades
Here you will find an overview of all our material grades, which we offer you in our standard programme. From hot work steel and case-hardening steel to powder metallurgical steel and carbide.
Read moreDesky a tyče Die sets Vestavné díly
SP - Precision die sets
In our precision die set, the guide pillar is fitted to the backing plate, which ensures optimum transfer of shear forces onto the guide system. It is available in sizes 196 196 to 496 696.
Read moreDesky a tyče Die sets Vestavné díly
SV-Standard die sets
Our tried and trusted SV standard die set is available in sizes ranging from 156 156 to 696 1396.
Read moreOffset cutting punches
With the offset cutting punches from Meusburger there are many possibilities to configure the contour of the cutting punches individually according to your needs. In addition, different materials and head shapes as well as coatings are available.
Read more