A few examples of our commitment to sustainability
Power generation
Since 2021, we have been purchasing electricity that is generated 100% from renewable energy sources.
Heat pumps and photovoltaics
Our Hohenems and Lingenau sites are heated and cooled completely without fossil fuel energy sources via heat pumps using 100% green electricity. Our new office building in Hohenems, which opened in 2022, also saw the arrival of the first photovoltaic system. 96 modules with an output of 35.5 kWp generate around 35,000 kWh of electricity per year. The system in Lingenau with 1144 modules and an output of 463 kWp was then put into operation in May 2023. This yielded 300,000 kWh in the first half of 2023. The photovoltaic system in Wolfurt was also gradually completed by the end of November 2023. The energy here is generated by 2776 modules. This is expected to yield 1.2 million kWh of electricity per year and covers around 7% of our electricity requirements.
Electricity savings
We save energy through various measures, such as LED lighting and detection of compressed air leaks as well as automatic shutdown of machines and systems. In addition, we strive to implement further optimizations on an ongoing basis.
Heat recovery
We do not waste any energy, but use the waste heat produced by our machinery and equipment for heating our plant. For example, our building at headquarters in Wolfurt is heated 90% with waste heat and only 10% with natural gas.
Cooling energy optimization system
We invest in highly efficient cooling systems on the rooftop of our production halls.
Separation of recyclables and waste
At Meusburger, all waste is meticulously separated into recyclables and residual waste, which enables environmentally sound recycling.
Filtering pollutants
To a large extent, our production process is pollutant-free. Any pollutants that do arise when processing steel are absorbed by means of suitable filtration devices.
Company bikes
Employees have the opportunity to obtain a subsidized bike for private and business use through Meusburger. Company bikes are also available at the Wolfurt and Hohenems train stations so those traveling to work by train can use them to cover the distance between the train station and the workplace.
Charging station for electric bikes
Employees who ride their electric bikes to work make a great contribution to the environment and can charge their bikes for free at one of our two charging stations. Charging stations are also available on the premises for our electrically powered company vehicles.
Biking contest
Every year, Meusburger takes part in the biking contest organized by the state of Vorarlberg. It encourages our staff to improve their health and at the same time protect the environment by using their bikes as much as possible. Further information
Staff transportation
41 minibuses are provided for our staff for traveling to work every day. Meusburger takes part in the klimaaktiv mobil project making an active contribution to environment and climate protection. Since 2022, the company minibuses are gradually being replaced by electric buses.
A habitat for bees
The bee is one of the most important organisms in our ecosystem. That’s why we helped young beekeeper Florian Faißt acquire his eight beehives, each with around 50,000 bees, and house them at our production site in Lingenau. The bees have plenty of blossoms in the flower meadow around the building and this allows us to make an active contribution to the preservation of biodiversity.