Flexible clamping is guaranteed by the pull-down oscillating jaws, and even awkward electrode blanks can be clamped without preparatory work. The HER 1144 is also suitable for light machining operations as well as subsequent machining of workpieces during wire EDM. Due to the ITS-50 interface, repeatable clamping is guaranteed.
![](/ZH/CN/media/PIC_PRO_SNG_Zentrischspanner-Beschriftet_INT.png)
See for yourself in the product video below, where you can also find tips on maintenance and installation.