Contacto

Estaremos encantados de atenderle en persona de lunes a viernes desde las 8:00 hasta las 17:00 horas. Haga clic en este enlace para buscar el interlocutor que le corresponde por zona.

Sede de Wolfurt
+43 5574 6706-0

Sus contactos

Carrito de la compra {{ (warenkorbCtrl.warenkorb.bestellNummer ? (' [' + warenkorbCtrl.warenkorb.bestellNummer + '] ') : '' )}} | {{warenkorbCtrl.warenkorb.items.length}} artículos   Cambiar de carrito de la compra

Observaciones

Imagen artículos Unidades Precio por unidad Precio total Precio total con descuento
{{warenkorbItem.produktgruppe.produktname}}

{{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben:[{attrPrefix: 'L_', searchPattern: '/...', replacePrefix: '/', replaceSuffix: ''}] }} {{warenkorbItem.bezeichnung | artikelBezFilter:warenkorbItem.attributwertEingaben}}

{{attributwertEingabe.attributBezeichnung}}

     
{{hannexItem.Benennung}}

{{hannexItem.Bezeichnung}}

     

Inicie sesión para ver los precios que se le aplican y continuar con el pedido.

Notas de prensa sobre Meusburger

¿Le interesan nuestra empresa y nuestros productos? Entonces está en el lugar adecuado.

Exclusive guide for inclined pin from Meusburger

03.10.2017, Fabricación de moldes

The exclusive E 3064 Guide for inclined pin stands out due to optimal surface contact with the inclined pin and best material pairings. This results in a high force absorption. The machining of the pocket in the slide is possible without inclining. In addition the slide stroke can be adjusted subsequently by customising, or adjusting the position of the guide for inclined pin.

 

During the entry of the inclined pin as well as when the mould is opening, the highest forces act on the surface between the inclined pin and the slide. In addition the inclined surface machining of the guiding hole in the slide is often very laborious. That is why Meusburger developed the E 3064 Guide for inclined pin. This is inserted in the slide and forms the contact surface for the inclined pin. Due to the special geometry in the hole, full-surface contact between the inclined pin and the guiding is created. Combined with the best material pairings, this leads to a higher force absorption. The introduction of the guide for the inclined pin is simple: you just cut a rectangular pocket with a threaded hole in the slide and then provide the required clearance for the inclined pin. Thus the machining can also be carried out on a conventional 3 axle machine and before the hardening. Furthermore it is possible to execute the installation conveniently from the split line face. The E 3064 Guide for inclined pin is available from stock for inclined pins with diameters of 12-30 mm. The CAD data including installation spaces is readily and easily available in our web shop.

 

Volver al índice de notas de prensa

Press contact

Should you require further information on this press release or have any questions or comments, please feel free to contact us by email.

Susanne Zukowski
Comunicación/RR.PP.

+43 5574 6706-1736

Dirección de correo electrónico

Iniciar sesión

¿Ya se ha registrado como cliente en el portal de Meusburger?

Si ya dispone de datos de acceso para el portal de Meusburger, inicie sesión aquí:

¿Ha olvidado la contraseña?

Ya hemos enviado la contraseña que acaba de crear. Debería recibirla en breve en su bandeja de entrada. ¡Qué tenga un día provechoso!

Introduzca una dirección de correo electrónico y
le enviaremos una contraseña nueva.

Seleccione su país

Filiales

Pruebe la nueva versión de Mi cuenta

Familiarícese de antemano con la nueva sección «Mi cuenta» y disfrute sus numerosas ventajas.

Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Familiarícese de antemano con la nueva sección «Mi cuenta» y disfrute sus numerosas ventajas.

Ahora, la nueva versión de «Mi cuenta» le permite también hacerse una idea general del siguiente nivel del portal de Meusburger. Puede ver toda la información y las ventajas del portal aquí.

Recordar selección
Beta
Nueva versión
Versión actual